Source

Associated with: WITS Application programs.

 

The Source attribute shows the location of the application program.

 

The location information has the following format:

Master <DNP3 Local Address>: OS <Outstation Address>: Program <Program Point Number>.

 

For more information, see Source.

You can specify the application program's location by using settings on the Application Program tab within the Application Program form ((see Configuring a WITS Application Program)).


Disclaimer

Geo SCADA Expert 2020