Supports WITS Version

Associated with: WITS Device Profile.

The Supports WITS Version attribute shows the version of the WITS standard to which the device profile relates. The Field Device may also support WITS versions that are earlier than this version (see Geo SCADA Expert WITS Version Support). The format for the version number is <major>.<minor>.

 

1.1

You can find details of the supported WITS version in the Device Identification section of the device profile (see Display a WITS Device Profile).

A Field Device has a set of WITS device attributes that Geo SCADA Expert reads whenever it establishes communications with the Field Device. The WITS Major Version (ID:1) and the WITS Minor Version (ID:2) attributes should match the Supported WITS Version attribute in the device profile. If the versions do not match, it means that you are using the wrong device profile.


Disclaimer

Geo SCADA Expert 2020