Trend Settings for WITS Maximum Points
You can display the trend, or movement, of the value of a WITS Maximum Point in the form of a graph.
The WITS Maximum Point is a type of analog point. Therefore, many of the fields in the Trend section of the Maximum tab are the same as those for other WITS analog points.The Maximum, Minimum and Logarithmic field values are inherited from the parent point (see Define an Analog Point's Trend Settings).