ApplyScaling
Description
This value indicates whether Wonderware Historian applies scaling to the analog tag. Wonderware Historian scales raw values to engineering units by using linear interpolation between the end points. As Geo SCADA Expert exports data that has already been scaled, additional scaling by Wonderware Historian should not be required. If the value for this property is set to True, then Wonderware Historian applies scaling. Therefore, the value for this property should be set to False.
Geo SCADA Expert Metadata Field
WH_ApplyScaling
Default Value
The default value for the property is False.
Type
Boolean.
Further Information