EngineeringUnit
Description
The unit of measure for an analog tag. For example: mph, grams, or pounds.
Geo SCADA Expert Metadata Field
WH_EngineeringUnit
Default Value
This will usually be the Units configured for the point or accumulator. For points that don't have units (for example, digital points) the default is an empty string.
Type
String.