RolloverValue

Description

The rollover value for the tag. The rollover value applies to tags associated with a counter device. The rollover value is the first value that causes the counter to roll over. Wonderware Historian uses this value for the counter retrieval mode. For example, for a counter that counts from 0 to 9999, the counter rolls over back to 0 for the 10,000th value it receives. Therefore, you would set the rollover value to 10,000. This property applies to analog tags.

Geo SCADA Expert Metadata Field

WH_RolloverValue

Default Value

The default value is 0.

Type

Double.


Disclaimer

Geo SCADA Expert 2020