StorageRate

Description

The rate at which Wonderware Historian stores the tag value if the storage type is Cyclic. This property applies only to analog tags. In Geo SCADA Expert the TagStorageType is always set to Forced, and therefore this property is not applicable.

Geo SCADA Expert Metadata Field

WH_StorageRate

Default Value

The default value for this property is 0.

Type

Unsigned Long.


Disclaimer

Geo SCADA Expert 2020