Store/Forward State

Associated with: Wonderware Historian database item.

If the store-and-forward cache is disabled then Geo SCADA Expert will not display this attribute.

The Store/Forward State attribute indicates the status of the HCAL store-and-forward cache.

The possible store-and-forward cache states are as follows:

For information on resolving anomalies, see Troubleshooting Wonderware Historian Driver Operation.


Disclaimer

Geo SCADA Expert 2020