TimeDeadband
Description
The storage time deadband for the tag. The time deadband is the minimum time, in milliseconds, between stored values for a single tag. Wonderware Historian will not store any tag value changes that occur within the time deadband. The time deadband applies to Delta storage only. A time deadband of 0 indicates that Wonderware Historian will store the tag value each time it changes. This property applies to all tag types. In Geo SCADA Expert the TagStorageType is always set to Forced (never Delta), and therefore this property is not applicable.
Geo SCADA Expert Metadata Field
WH_TimeDeadBand
Default Value
The default for this property is 0.
Type
Unsigned Long.