Configuring X-Y Plots

Each X-Y Plot is represented in the database by an X-Y Plot database item. These items store the configuration settings for the X-Y Plots that define:

To create an X-Y Plot item and configure it so that it contains the information you require:

  1. Create an X-Y Plot Item
  2. Display an X-Y Plot in Design Mode
  3. Edit an X-Y Plot Item
  4. Configure the X-Y Plot Database Item Properties.

After configuring an X-Y Plot, you can proceed to view it in Run mode (see Using X-Y Plots).


Disclaimer

Geo SCADA Expert 2020