Common Advanced Driver Log File Options

Driver Logging can be used to help diagnose abnormal conditions relating to driver activity. Driver logging can also be used for assessing potential problems. The log files that are produced provide useful diagnostic information about specific aspects of the system. For example, the Points logging option provides diagnostic information about the points on a particular driver.

Should you need to contact Schneider Electric for assistance with resolving a problem that Geo SCADA Expert has detected, you might be asked to provide Log files to help in assessing the cause of the problem. Be aware that existing warranty and support arrangements determine the level of help that you receive should you need to contact Schneider Electric.

This section explains the driver logging options that are common to many advanced drivers.

Those driver logging options that are typically required for investigating abnormal conditions are enabled by default. We suggest that the logging options are left at this default unless other logging options are specifically requested by Schn, or the default options are adversely affecting system performance.

For information on any driver logging options that are not listed below, see the driver-specific documentation.

These driver log file options are common to many advanced drivers:

Application

Logs general information about the driver.

Errors

Logs any errors detected during driver operation. For example, a loss of connection to the Geo SCADA Expert database.

Timers

Logs information about low-level internal thread timer queues.

ATTENTION: The Timers option typically logs a large amount of information. As such, we recommend that this option is only enabled if specifically requested by Schneider Electric engineers.

Events

Logs information about low-level internal thread event queues.

ATTENTION: The Events option typically logs a large amount of information. As such, we recommend that this option is only enabled if specifically requested by Schneider Electric engineers.

I/O

Logs information about low-level I/O.

Database Objects

Logs configuration changes to database items (any create, delete, or modify activity on the system).

Channels

Logs general information about the channels on the system, including the channel’s state, and activities including attaching or detaching outstation sets.

Outstation Sets

Logs general information about the outstation sets on the system, including one shot, promoted dial out, and channel switching.

Outstations

Logs general information about the outstations on the system, including the outstation’s state, current channel, and any switching activity.

Points

Logs general information about the points on the system, including controls and persistence.

Modems

Logs information on dial-up modem exchanges and states.

Scanners

Each channel has a scanner that is responsible for scanning the outstation(s) on that channel. The Scanner Log File option logs information about each scanner.

Requests (Actions)

Logs information about any external requests from users, plus internal requests within the driver.

Point Updates (Data)

Logs information about point data retrieved by the driver.

Scanning Phases

Logs information about the phases of outstation scanning (primary, secondary, promoted, exception, and so on).

Client Sink

Logs information about the low-level interface from server to driver.

Server Sink

Logs information about the low-level interface from driver to server.

Browse Server

Logs information about the use of the browse options on configuration Forms.

Server Sink Lock

Logs information about the time taken to perform individual server requests. This includes how long a driver thread waits for the local driver sink lock, how long the database takes to process the request, and the total time taken to complete both activities.

Further Information

Log files and Log file settings: see Driver Logging.

Displaying log files: see Display a Driver Log File.

The log file options to turn on if experiencing problems with an advanced driver, see Troubleshooting.

Types of log file supported by Geo SCADA Expert: see Logging and Monitoring.


Disclaimer

Geo SCADA Expert 2021