Number of Points

Associated with: Dynacard Stores

This status attribute indicates the number of data measurements (‘points’) contained in the particular set of dynacard data to which the attribute relates.

Use the status attribute in conjunction with the relevant <Dynacard Type> Dynacard and Outstation Timestamp status attributes.

Example:

Reference Dynacard: 12/Jun/2012 16:46:33.344
Number of Points: 128

(Indicating that the ‘Reference’ Dynacard data that Geo SCADA Expert uploaded at 16:46:33.344 on 12th June 2012 contained 128 dynamometer measurements.)

To view a plot of the data comprising the above measurements (‘points’), display the relevant Dynagraph (see Dynagraphs).


Disclaimer

Geo SCADA Expert 2021