Preparation - PSTN Channels

You need to add an appropriate PSTN Channel for each telephone line that is used on your system.

To configure a PSTN channel, you need to have access to details of the outstation’s dial-up modem settings.

Often these settings are fixed, according to the type of dial-up modem being used. Refer to the documentation associated with the modems for these settings—you need to configure each PSTN channel to have the same settings as the modem with which it is associated.

Where any settings are not fixed, you need to be aware of which settings are being used for the dial-up modems on your system. The engineers that configure the outstations should create a list of the settings that they have configured. If you have access to such a list, you can use it to define those requirements.

In addition to the dial-up modem settings, you also need to know the:

You can configure each PSTN channel to use a variety of features, including Alarm Redirection, and Alarm Views. However, many of these features are optional and do not affect the success of communications between the Geo SCADA Expert server and the outstations. The optional features include:

If the features listed above are not configured, they are not used for the selected PSTN channel (they will be left blank).


Disclaimer

Geo SCADA Expert 2021