Show or Hide a Trace or its Markers

You can choose to show or hide any of the traces that a Dynagraph is able to display. You can also choose to show or hide the markers that are assigned to a trace.

To show or hide a trace or its markers:

  1. Display the Dynagraph in Run or Design mode, as required (see Displaying an Editor).
  2. Right-click on the key at bottom of the Dynagraph.
    A context sensitive menu is displayed.

  3. Use the menu options to specify whether you want to:
    • Display or hide the Markers for that particular trace
    • Display or hide the Trace (you can also do this by selecting or clearing the check box that is displayed to the left of the trace information)
    • Display the traces for All available dynacard data that the Dynagraph is designed to show.
    • Display None of the Dynagraph’s traces.

Disclaimer

Geo SCADA Expert 2021