Specify the Length of Time that a File Upload Report is Retained on the Server

Use the Historic tab of the File Upload Form to specify the amount of time for which any report that is associated with the uploaded data, is retained on the server.

The Historic tab is only included on the relevant configuration Forms when the Historic Files feature is enabled on the server. The Historic Files feature enables Geo SCADA Expert to store files such as reports historically (see Enable or Disable Historic Files).

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value. For example, enter 4W for a report to be retained for a four-week period.

Operators can display the reports using the Display Report pick action. (Where more than one report is stored on the server, a window is displayed, allowing the required report to be selected.)


Disclaimer

Geo SCADA Expert 2021