Define the Point Scaling

Use the fields in the Scaling section of the Analog Input Point Form to specify the type and range of the raw input signals, so that they can be suitably converted into floating-point engineering values for use in the Geo SCADA Expert database.

Conversely, use the section on the Analog Output Point Form to perform a similar conversion on any output signals. Geo SCADA Expert uses the conversion calculation to produce a raw data value that is sent to plant.

There are two levels of scaling that can be applied to an analog point. The first level is scaling a raw value into an engineering value using linear interpolation. This level of scaling is applied only if the controller is configured to return an integer value. This level of scaling is disabled when the controller is configured to return a floating point value.The second level of scaling is where the Multiplier and the Offset values are applied. This second level of scaling is always applied.


Disclaimer

Geo SCADA Expert 2021