Which Driver?

For Geo SCADA Expert to communicate with 'Generic' Modbus controllers using the Modbus protocol, use either the 'Generic' Modbus database items with Geo SCADA Expert’s Advanced Modbus driver, or the Simple Modbus driver. The Advanced Modbus driver supports additional functionality to the Simple Modbus driver, including:

For certain types of Modbus controller, Geo SCADA Expert uses an Advanced Modbus Extension Driver to provide vendor-specific functionality for those devices. For further information, see the relevant Advanced Modbus extension driver guide.

For information about the Simple Modbus driver, see the Geo SCADA Expert Guide to the Simple Modbus Driver.

If both drivers provide the required functionality, consider using the Advanced Modbus driver rather than the Simple Modbus driver. Using the Advanced Modbus driver will give you more flexibility should your system requirements change in the future.

Further Information

Supported Drivers and Protocols.


Disclaimer

Geo SCADA Expert 2021