Configure Alarm/Event Logging

The Alarm / Event Logging section of the Server tab allows you to specify the Severity and the Area of Interest of alarms and events associated with the state of the connection to the OPC DA server and the state of the OPC DA server itself.


Disclaimer

Geo SCADA Expert 2021