Associated with: Advanced OPC Groups
Security permission required to access this pick action: Switch Line
Use the Switch Server pick action to switch the server that the Advanced OPC Group is currently using.
When you use the Switch Server pick action the Switch Server window provides a list of servers between which the Group can be switched.
                 
            
The current server is selected by default. Choose the new current server for the group then select the OK button.
If you attempt to switch to a server where the connection state for that server is not 'Healthy', then the selection is rejected.
NOTE: If using this pick action with the Automation Interface, you have to specify the method name SwitchServer.