Specify the Stream Identifier that Prefixes Messages Sent to and from the Radio

Use the SID Code field on the Radio tab to specify the SID code that is to be included in the header of the messages transmitted to and from this radio.

This field only applies if the Send SID check box is selected on the configuration Form of the Trio Diagnostics Radio Set that is associated with the radio (see Specify Whether to Include the Stream Identifier in each Data Packet).

In many cases, you can leave the SID Code at the default of 0 (zero).

If the configuration in the radio has been modified, use the SID Code field to specify the diagnostics SID code that is configured in the radio unit.

For information on SID codes, and how to configure the radio to control how the messages are routed, see the documentation supplied with your Trio radio equipment.


Disclaimer

Geo SCADA Expert 2021