Add a User Roster

To add a User Roster:

  1. Right-click on the System or Group to which you want to add the roster (this might be a separate group for storing redirection actions, or for storing user details).
    A context sensitive menu is displayed.
  2. Select the Create New option.
    A further menu is displayed.
  3. Select the Alarm Redirection option.
    A further menu is displayed.
  4. Select the User Roster option.
    A User Roster is added to the system. It is selected automatically, ready for you to enter its name.
  5. Enter a suitable name for the User Roster (see Naming Restrictions in the Geo SCADA Expert Guide to Core Configuration).
  6. Select another part of the interface or press the ENTER key to confirm the entry.

When you have added a User Roster, you need to Configure the User Roster Properties.


Disclaimer

Geo SCADA Expert 2021