Specify the File Description Information that is Exported

Use the fields within the File Description section of the CFX Export tab to specify the descriptive information that is exported with flow measurement data. The CFX Header is included in each exported file’s header, whereas the Meter Number, Meter Name and Serial Number are typically included at the start of the configuration section in each export file.

 


Disclaimer

Geo SCADA Expert 2021