DB Client Logging

DB Client log files contain low level information about the connections between the client(s) (other than ViewX) and the Geo SCADA Expert server. This includes information about each request made by the client and the responses received by the client. DB Client log files are useful when investigating problems with client-server connections.

There are two groups of DB Client log files:

To enable or disable DB client logging, you need to configure the logging settings via a registry editor (see Using a Registry Editor to Change Client Log File Settings).

To display a client log file:

  1. Use Windows Explorer to locate the log file. The log files are stored at the location that is specified in the LogFileBase registry setting.

    The default location of the LogFileBase registry setting is:

    HKEY_CURRENT_USER\SOFTWARE\Schneider Electric\ClearSCADA\DBClient\LogFileBase

    (If the log file is not at this location, a different path might be specified in the registry (see Using a Registry Editor to Change Client Log File Settings).)

  2. Open the log file in a text editor program, for example, Microsoft Windows Notepad.

Disclaimer

Geo SCADA Expert 2021