Define the Name for the Data Source

When you create a connection between a Geo SCADA Expert system and a Third Party ODBC Client, you need to specify a name for the data source. You will be able to use the name you enter to identify the connection.

You can enter any name, but we recommend that the name you use makes it easy for other users to identify the connection too.

To define the Data Source Name (DSN), display the ODBC Setup window Configure the ODBC DSN Settings, then enter the required DSN in the Name field.


Disclaimer

Geo SCADA Expert 2021