Firewall Settings for Client - System and Server Advise Connections

If you are configuring a firewall that will be used on a client - system connection, you should check that the firewall:


You can ignore the information in the rest of this topic if all of the clients and servers on your system are running Geo SCADA Expert 2020 or later versions of the software. The Sockets button, Sockets window, and port range for advise links only apply when one or both ends of the connection (server or client) are running a version of Geo SCADA Expert that is earlier than Geo SCADA Expert 2020.

If either end of the connection (server or client) is running a version of Geo SCADA Expert that is earlier than Geo SCADA Expert 2020, you should also check that the firewall:

For more details on configuring a firewall, please refer to the documentation supplied with your firewall product.


Disclaimer

Geo SCADA Expert 2021