ViewX clients provide access to Geo SCADA Expert's configuration and operation features (although security permissions can be used to restrict access to them). Each ViewX client has two communication links to the Geo SCADA Expert server, both of which are set up when you create a ViewX client - System connection.
In the following sections, we describe how ViewX clients communicate with the Geo SCADA Expert server and explain how to configure the connection and firewalls. We also provide information on checking the status of the connection.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
To avoid potential DCOM issues, ViewX clients use Data Access Components to communicate with the Geo SCADA Expert server using the TCP/IP protocol. The Data Access Components are installed on the ViewX client automatically when you install ViewX.