ViewX Command Line Arguments

You can use ViewX command line arguments to pre-set the settings for ViewX. The ViewX commands are:

You can enter these commands at a Windows command prompt or you can configure desktop shortcuts that include the commands as part of their Target.

You can use combinations of ViewX commands: precede each command with the / character and separate the commands with a space. For example, /Instance:2 /Systems:"E:\SystemsCPLX2.xml."


Disclaimer

Geo SCADA Expert 2021