Working with Single and Multiple Databases

A ViewX client can be configured to access a single Geo SCADA Expert database or multiple Geo SCADA Expert databases. Each Geo SCADA Expert database is independent and runs as a Geo SCADA Expert system on a Geo SCADA Expert server (or on multiple Geo SCADA Expert servers if used in a multi-server redundant architecture). This means you can use a single ViewX client to:

For more information on single and multi-database setups, please refer to the following sections:

A ViewX client can connect to a maximum of 64 databases.


Disclaimer

Geo SCADA Expert 2021