Abstract Item

You can add ‘core’ or driver-specific items to a Group Template—such items are then replicated in each Group Instance that references the Group Template. In addition to ‘core’ and driver-specific items, you can optionally add Abstract Item(s) to a Group Template.

All of the items that appear in the Group Template are replicated within each Group Instance. Within each Instance, Abstract items that are required in that Instance can be converted into the required type of point or outstation. (Any Abstract items that are surplus to requirements in a particular Group Instance are left unconverted and are effectively ignored by Geo SCADA Expert.)

You might decide to use Abstract items when, for example:

For an example further demonstrating how Abstract Items might be used on a system, see Convert an Abstract Item into a Specific Type of Point.


Disclaimer

Geo SCADA Expert 2021