Add a Parameter

To add a Parameter to the Geo SCADA Expert database:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the System or Group for which you want to add a new Parameter.
    A context sensitive menu is displayed.
  3. Select the Create New option.
    A further menu is displayed.
  4. Select the Parameter option.
    A further menu is displayed.
  5. Select the required option from the list.
  6. A Parameter of the corresponding type is added to the root of the System or to the selected Group (depending on your selection in step 2). It is selected automatically, ready for you to enter its name.
  7. Enter a suitable name for the item (taking into account the Geo SCADA Expert Naming Restrictions).
  8. Press the Enter key or select another part of the ViewX interface to confirm the entry.

Once you have added a Parameter, you need to configure its properties (see Configure a Parameter).


Disclaimer

Geo SCADA Expert 2021