Add an Action to a Schedule

With any type of Schedule, you need to specify the action(s) that Geo SCADA Expert is to perform automatically at the scheduled time(s), and the database item(s) on which Geo SCADA Expert is to perform those action(s). You do this using the Add Action window. The database items and actions that you specify are then displayed in the Object and Action areas at the bottom of the Schedule Editor.

The procedure that you use to assign the action trigger times differs, depending on the type of Schedule:

There are two means by which you can specify the action(s) that Geo SCADA Expert is to trigger automatically at the time(s) indicated on a Schedule. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021