Configuration Changes and Structure Changes

The Configuration Transaction feature is designed to stop you from making changes when an update is pending. With items in Group Templates and Group Instances, these changes include alterations to the configuration of items and changes to the structure of the database (see Activities that are Restricted when Configuration or Structure Changes are Pending).

The operations that are referred to as Configuration Changes are:

The operations that are referred to as Structure Changes are:


Disclaimer

Geo SCADA Expert 2021