Delete a Scheduled Action

If an action that is associated with a Schedule no longer needs to be triggered by that Schedule:

  1. Display the Schedule in Design Mode.
  2. Either:
    1. Right-click on the action in the Object area of the Schedule Display.
      A context sensitive menu is displayed.

    2. Select the Delete option.

    Or:

    1. Select the action in the Object area of the Schedule Display.
    2. Press the Delete key.

    The obsolete entry is removed from the Schedule Display.

  3. Save the configuration.

Disclaimer

Geo SCADA Expert 2021