Edit a Data Table

To edit a Data Table, so that you can specify the fields that you want to include in the table, you have to display the Data Table in Design Mode. To do this, either:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Double-click on the Data Table in the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature enabled).
    The Data Table is displayed in Design mode.

or:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. Right-click on the Data Table in the Database Bar.
    A context sensitive menu is displayed.
  3. Select the Edit Data Table option.
    The Data Table is displayed in Design mode.

You can perform various editing activities when a Data Table is displayed in Design mode. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

Keyboard Shortcuts

Configure the Properties on the Data Table Form.


Disclaimer

Geo SCADA Expert 2021