Logging

Associated with: Channels

The Logging state is indicated by a dark yellow background color, by default.

The color indicates that Communications, I/O, or Telnet logging is enabled for a channel. When this feature is enabled, the communications between the Geo SCADA Expert server and the outstations that are using the channel are logged to a text file.

For information on Channel Communications logging and I/O logging, see Communications Logging. For information on Telnet logging, see Telnet Monitoring.


Disclaimer

Geo SCADA Expert 2021