Numeric Syntax

The syntax for numeric values is given below.

Code Description

.

Decimal point

,

Separator (for instance to separate 1000s)

‘

Insert a single quote at start and end of any string to indicate plain text

%

Multiplies the value by 100 and displays it as a percentage

E

Use in scientific notation to separate the mantissa and the exponent (for example, #E+00)

#

A digit (omitted if zero)

0

A digit (still displayed, even if the value is zero)

Example:

Using the syntax #,### results in the value 1000000 being displayed as 1,000,000 (the separator automatically repeats for each occurrence of three digits—there is no need to include a further separator)

Using the Custom syntax 0E0 results in the value 900 being displayed as 9E2

A value formatted using a Number category format with two digits after the decimal place appears as .75

To display a leading zero before the decimal point, use the custom syntax 0.## (or 0.00 to always display two digits after the decimal place)

The value then appears as 0.75

Using the Custom syntax #% results in the value 0.75 being displayed as 75%

The Custom syntax ‘Weight: ‘ 0.## results in the value 0.75 being displayed as
Weight: 0.75.


Disclaimer

Geo SCADA Expert 2021