Specify the Frequency with which Geo SCADA Expert Stores Timed Report Values

Geo SCADA Expert can log Accumulator data by Timed Report, whereby the server regularly stores Accumulator values in the database, regardless of whether those values have changed. Use the fields within the Timed Report section of the Reset tab to specify when Geo SCADA Expert logs Accumulator values on a Timed Report basis. Use the Continuous check box at the top of the Reset tab to specify whether Timed Reports still occur when an Accumulator has no new data to process (see Specify whether an Accumulator Continuously Sends Timed Reports and Resets its Value).

Example:

An Accumulator has this Timed Report configuration:

Interval: 5M
Offset: H
Local Time check box: Checked (End of Period resets are calculated using Local time)
Daylight Saving Time: Checked (Geo SCADA Expert automatically adjusts the time to take into account any DST adjustments).

Geo SCADA Expert logs the Accumulator value on the hour, and then at five-minute intervals throughout the day, taking account any DST adjustments.

If the Accumulator’s Continuous check box is not selected (see Specify whether an Accumulator Continuously Sends Timed Reports and Resets its Value), and there are no source values to process for part of the time, those Timed Reports will not occur until the next source value is processed, whereupon Geo SCADA Expert will calculate the ‘missing’ Timed Reports and populate its historic database with those report values (time stamped with the times at which they would have occurred if data had been available for processing).

Use the Timed Report check box in the Historic Data Filter section of the tab to specify whether Geo SCADA Expert is to store the Accumulator's Timed Report values historically (see Specify the Data that Geo SCADA Expert Stores for an Accumulator).


Disclaimer

Geo SCADA Expert 2021