Specify the Period over which an Accumulator’s Value is Calculated

Use the fields within the End of Period Reset section of the Reset tab to specify the period over which an Accumulator’s value is calculated. Use the Continuous check box at the top of the Reset tab to specify whether End of Period Resets still occur when an Accumulator has no new data to process (see Specify whether an Accumulator Continuously Sends Timed Reports and Resets its Value).

Example:

An Accumulator has this End of Period Reset configuration:

Interval: 1H
Offset: D
Local Time check box: Clear (End of Period resets are calculated using system time).

The Accumulator monitors its source value from 00:00hrs each day for a one-hour period. At the end of this period, the Accumulator value is reset to zero. The Accumulator then monitors its source value for another one-hour period, before the Accumulator value is again reset to zero. This activity is repeated throughout the day, with the last calculation period starting at 23:00hrs.


Disclaimer

Geo SCADA Expert 2021