Using Print Preview

Certain features, such as Function Blocks and Query Lists allow you to preview the printed output before actually printing. When you select the Print Preview option for a selected feature, the preview is displayed in the Document Display Area.

The Preview toolbar is displayed at the top of the preview display with the following commands:


Disclaimer

Geo SCADA Expert 2021