Variables

You can use some types of Variable in a similar way to internal Points. Like internal points, Variables only exist within the master station software. You can use Variables in Logic programs, Value Maps, and so on. However, unlike internal points, Variables do not have the additional ‘overheads’ associated with points, such as the ability to generate events or alarms.

Create and configure a Variable on your system if you require:

Consider using an Array Variable, rather than a single-value Variable, if a series of values are required.

For more information on Variables and Variable arrays, see Using Variables to Store Data Values.


Disclaimer

Geo SCADA Expert 2021