Overview of a Digital Point’s Trend

Each Trend consists of an x-axis, a y-axis, and a trace. The x-axis displays a time interval, and the y-axis displays the point states. The Trace represents the digital point’s current or historic state.

You need to define the values of the Trend’s x-axis, to determine the time period over which the point’s states are shown, so that a suitable range of units are displayed.

To do this for a Current Trend, you need to use the fields in the Trend section of the Digital Point Form’s Digital Point tab (see Procedure for Configuring the Settings for a Digital Point’s Current Trend).

For a Historic Trend, you need to use the fields on the Digital Point Form’s Historic tab (see Define the Time Period Shown on Historic Trends and Lists).


Disclaimer

Geo SCADA Expert 2021