Using Calculation Point Specific Actions

Geo SCADA Expert supports a wide variety of operator-driven or automated actions and controls. When performed by an operator, the actions are typically selected from a context sensitive pop-up menu (see Object Menu in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients).

This section covers the Execute action that is specific to calculation points.

The pick actions in ViewX and Virtual ViewX represent just some of the methods that are available to use. To find out about other methods that are available for each type of database item, please refer to the Database Schema (see Working with the Database Schema in the Geo SCADA Expert Guide to the Database). The Database Schema also provides details on the name and arguments of each method, so that you can call the methods from your own programs and scripts.

Users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).

Further Information

‘Core’ pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.

Pick actions that are common to items on many drivers: see Actions that are Common to Many Drivers in the Geo SCADA Expert Guide to Drivers.


Disclaimer

Geo SCADA Expert 2021