Define the Print Properties

Use the fields within the Printing section of the Crystal Report tab to define the settings that are used when printing a report using the Print Report pick action. This pick action allows you to print a report using data obtained directly from the database.

(If you print a report directly from the Crystal Reports application, you need to specify the print setup from within the Crystal Reports application, rather than on this Form. If you use the Crystal Reports Viewer to display a previously generated report in ViewX, and then choose to print that report, you can specify the print settings using the Print option, available from the ViewX File menu. You then use ViewX’s Print menu option to print the report. (For more information on the latter, see Using the Crystal Reports Viewer.))

When defining the printing options, remember that the settings you choose have to be supported by the printer(s) on your system.

You also need to Define the Page Margins for any printed reports.


Disclaimer

Geo SCADA Expert 2021