Formula Field

You can use Formula fields to include data that does not exist in any Geo SCADA Expert database fields. By writing a formula, you can calculate additional data that you want to use or display in a report.

You typically write formulas using Crystal syntax—for information, see the documentation provided with the Crystal Reports application. For examples of how a formula (rather than a Formula field) can be used in a report, see Point Listing that Uses Color to Indicate Alarm Status, and see Restrict the Amount of Data that is Queried in a Report.

When writing formulas, use the Check button to test that the syntax is correct.

As an alternative to using formulas in Crystal Reports, you can use Data Grids to specify the information that you want to include in a report. A Data Grid is in effect a ‘custom’ table. Geo SCADA Expert can perform a variety of calculations on the data in a Data Grid and display the results of those calculations in the report. For further information, see Configuring Data Grids in the Geo SCADA Expert Guide to Core Configuration. For an example of how a Data Grid can be used in a report, see Embedded Data Grid Content.

Further Information

Add a Field to a Report.

Custom Fields in Reports.


Disclaimer

Geo SCADA Expert 2021