To launch the Crystal Reports application from within Geo SCADA Expert, either:
- Double-click on the Report entry within the Database Bar (if you are logged on as a user that has the Double Click Edits Documents feature).
Or:
- Either:
- Right-click on the Report entry within the Database Bar.
- Select the required Report entry on a List.
- Select an animated representation of the report on a Mimic.
 A context sensitive menu is displayed.
- Select the Edit Crystal Reports option.
or:
or:
The Crystal Reports application window overlays the Geo SCADA Expert window (see Understand the Crystal Reports Work Areas).