DNP3

Configure Ethernet Keep Alive Polls

Use the fields within the Ethernet Keep Alive Poll section of the Direct tab to configure if, and how often, Geo SCADA Expert sends a periodic DNP3 Request Status of Link frame to the outstation. This transmission is designed to stop an Ethernet TCP/IP link from being disconnected by the Geo SCADA Expert server’s operating system, or the outstation, due to long periods of inactivity.


Disclaimer

Geo SCADA Expert 2021