DNP3

Configure Logged Data Properties

On DNP3 outstations, you can log data historically for point types other than Pulse Actions. Whenever the Geo SCADA Expert DNP3 driver contacts an outstation, it retrieves point data that is stored at the outstation and processes that data.

ATTENTION: If you enable logging on this tab, you also need to enable logging on the Historic tab. The Historic tab defines how the Geo SCADA Expert server stores data historically.

Use the fields within the Logged Data section on the <Point Type> tab to specify which of this retrieved point data Geo SCADA Expert logs historically, and which data it processes to generate alarms:


Disclaimer

Geo SCADA Expert 2021