DNP3

Configure Override Properties

Use the fields within the Override section of the Analog Point tab to specify whether a point’s value can be overridden.

Many of the fields within this section are common to many analog points—for details, see Define whether an Analog Point can be Overridden in the Geo SCADA Expert Guide to Core Point Configuration. Fields that are specific to DNP3 points are explained below.


Disclaimer

Geo SCADA Expert 2021