DNP3

Configure Point Scaling

Use the fields within the Scaling section of the Analog Point tab to specify if, and how, Geo SCADA Expert scales the point values that are reported by the outstation.

ATTENTION: There are two levels of scaling that can be applied to a DNP3 analog point. The first level is scaling a raw value into an engineering value using linear interpolation. This level of scaling is applied only if the outstation returns integer values. At this level, if the outstation reports the value as a floating point value, Geo SCADA Expert ignores any configuration in the Raw Full Scale and Raw Zero Scale fields, regardless of the Enabled setting. The second level of scaling is where the Multiplier and the Offset values are applied. This second level of scaling is always applied.


Disclaimer

Geo SCADA Expert 2021