DNP3

Integrity Poll Statistics

Associated with: DNP3 master outstations

The Integrity Poll Statistics attribute shows the number of attempted and successful DNP3 Integrity Polls issued by the Geo SCADA Expert DNP3 driver to the outstation since the statistics were last reset.

You can reset the statistics using the Reset Poll Statistics pick action. If the poll statistics have been reset, two sets of Integrity Poll Statistics attributes are displayed. The first displays the statistics since the last reset of the poll statistics; the second displays the statistics between the previous two resets.

Example:

24 attempted, 23 successful since 04/Nov/2003 11:36:49.255

If the statistics have been reset, a second entry will display statistics in the form:

124 attempted, 99 successful between 04/Oct/2003 11:32:49.261 and 04/Nov/2003 11:36:49.255


Disclaimer

Geo SCADA Expert 2021